(0)| 4/19/2010 12:59 PM | |
|
Posts: 3609 Rating:
|
Import of a Technical Question of an User Ibrahim10 wrote: Hi again. Than you all for the comments and directives that have helped me a great deal. I now am able to connect and upload/download my TP170B devices wherever i find them in the factory. Going back to me initial problem. I have been directed to create an new project with the new OP i want to use as a replacement(OP177B). Then I am told I can now convert my old project into this new one before downloading into the OP177B. Problem now is that I cannot finf the OP177B in the "project wizard - device selection" menu of Protool so i cannot create its project. I have checked and seen that my OP177B is not an installed component of my PG's Protool.The highest OP is OP170B.What can I do to get the library updated with the OP177B so i can use it? I had a breakdown in our water treatment plant where the TP170B went balnk and out and needs replacement. Is there another special package called prosave?. |
Follow us on