(0)| 2/28/2011 6:39 PM | |
|
Posts: 206 Rating:
|
Hi Jiri, to your questions. 1. The produktion of the Siwarex U is not discontinued, the only a full compatible successor. It is also colles Siwarex U with a new orderr no. 7MH4950-*. Have a look to the Siwarex homepage www.siwarex.com. 2. Yes, ist is a S7-300 module. You can use it without restrictions. 3. The lenght of the cable can be up to 500m. Watch for EMC. http://support.automation.siemens.com/WW/view/en/23923799 4. Itis not passoble to "physicaly recalibrate" a load cell. You have to look at the data if the nominal load of the load cell matches to your needs. Anyway the Tedea 240 loadcells are single point load cells, these cells should be only used as single cells. If you have an application with more load cells you should use different cells. Regards ABenno |
| 3/1/2011 9:55 AM | |
|
Posts: 206 Rating:
|
Hello Jiri, there are two types of Siwarex U: The 7MH4950-1AA01 with one channel, for one scale and the 7MH4950-2AA01 with two cahnnels, for two scales. The best would be to by the new configuration package, because of the new Siwatool and integration in the HW-Catalogue. It is also possible to use the old configuration package, but you only have the old Siwatool, that is also working with the new modules and the old integration of the old modules. If you go to www.siemens.com/mall you can find the "Industry Mall" and there you can order. For more technical support for Siwarex you can also contact hotline.siwarex@siemens.com . Regards ABenno |
Follow us on