(0)| 5/7/2011 7:34 PM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello Tomy, For the moment all the info concerning new generation of LOGO! is there about new modules logo . After two months I think the situation will be clear. Best regards, Hristo Mihalev |
| 5/9/2011 7:54 AM | |
|
Posts: 2930 Rating:
|
Hi, I have seen this at Hanover fair this year. They have used WinCC flex 2008. As communication driver S7-200 was used. In LOGO! a Ethernet connection has to be configured with an Operator Panel (same like Simaitc). If you want to display FB parameter, then in LSC a VM-Mapping table has to be filled with the FB and the required parameter. On a Panel you can directly read: I, Q, M. Here I0.0 (Panel) is I1 (LOGO!). Check this file from the German LOGO! forum: /tf/WW/de/postattachments/download?attachmentId=19071&onlyInternet=False Hope this helps |
| 5/9/2011 9:36 AM | |
|
Joined: 5/4/2009 Last visit: 12/21/2025 Posts: 916 Rating:
|
OK! So there is not yet an official release of the software and its drivers. Regards. Tomy.
|
|
Aim Higher |
|
| 5/26/2011 8:50 AM | |
|
Posts: 495 Rating:
|
I have heard that the release of the new LOGO! 0BA7 is at the beginning of July. |
| 5/26/2011 9:13 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello,
Measn "LOGO! 0BA7 (means SoftComfort also) on summer 2011th (June/Juliy 2011th).". BTW in above mentioned links you could find avery useful info... Best regards, Hristo Mihalev |
Follow us on