(0)| 6/8/2007 2:58 PM | |
|
Posts: 1084 Rating:
|
please post in the wincc felxible conference next time. I have asked the moderator to transfer your post. with regards, Ikkezelf |
| 6/8/2007 6:54 PM | |
|
Posts: 1275 Rating:
|
Hi Techy, If you wish to display WinCC's screens in an HMI you can configure it as a thin client. Best regards, Danielle |
| 6/8/2007 8:47 PM | |
|
Posts: 57 Rating:
|
Could you explain a little more how thin clients work? |
| 6/8/2007 8:55 PM | |
|
Posts: 1275 Rating:
|
Hi, Thin client is a feature of the WinCC option Web Navigator. You can configure, for instance, an MP370 as a thin client, which will access your Web Navigator server: ThinClient solutionsThe Web Navigator can also run under Windows 2003 terminal services. A Windows 2003 Server (or higher) operating system is required. This makes it possible, for example, to connect even Windows CE-based visualization systems such as SIMATIC MP 370 with the ThinClient MP option, to WinCC. For this purpose, the Windows terminal services must be installed on the PC on which the Web Client is installed. A Windows 2003 Server (or higher) operating system is required. Up to 25 ThinClients can be connected to one terminal server. Applications:
You can find further info on Web Navigator on this forum, and also on this link. Best regards, Danielle |
Follow us on