(0)| 8/7/2008 2:13 PM | |
|
Posts: 1742 Rating:
|
Hello, Did you have a look to this manuals? http://support.automation.siemens.com/WW/view/en/9830806 Look at chapter 4 File ==> Projects ==> ... The following functions are available in the File menu. File >Project > Set F4. You can set all the parameters required for aspecific project. These include the following: – Files belonging to a project. These files are always set in the job and listboxes or dialogs in which they will be addressed. – Parameters, e.g. symbols, method of representation (LAD, CSF, STL),character set etc. Once you have selected the settings for a project, you can only edit this project. File >Project >Load... F10. All the settings for the selected project areloaded. Once the project is loaded, only the files belonging to this project can be selected for editing. File >Project > Save. All the settings are saved in the file for thespecific project. |
Last edited by: edr at: 8/7/2008 2:17 PM |
|
Follow us on