(0)| 1/14/2009 9:18 PM | |
|
Posts: 1690 Rating:
|
Hi MancesterPete, a look into the handbook and you can find most of your questions: No, a direct connect of this sensor is not possible, because - 5 V is to low - LOGO 12/24RC modules (and DM 12/24R) needs 8,5 V to detect a high-level; LOGO 24V needs 12 V to detect high-level! - the frequency is a little bit to high for the normal digital inputs (but some LOGOs can this detect right - test it) you need the high inputs of the 12/24 modules If you modify the input voltage (e.g. with a optocoppler or aphotoMOS-relais), you can use the LOGO. LOGO!-Circuitsto do this with 1 and 2 channals you can find from me her into the forum - look at my collection and for some here in the english forum part. Best regards Betel |
Follow us on