6/12/2023 12:41 PM | |
Joined: 7/19/2022 Last visit: 11/18/2024 Posts: 420 Rating: (71) |
Hello Nicolas P. The panel model you mention can be programmed with WinCC flexible Compact version 2004 or higher. You can see it in the technical data of said panel: |
If this Information really helps, you could use the Rate function |
|
6/12/2023 2:47 PM | |
Joined: 4/10/2020 Last visit: 11/4/2024 Posts: 77 Rating: (1) |
Hi JBS98, yes, thank you, but i do not have WinCC flexible Compact 2004. What i wonder is if the mention "or higher version" includes other version of WinCC flexible such as Wincc Flexible 2008. In WinCC Flexible 2008 SP3, I can add a TP170A, I guess that it means that it would be compatible, but i just wanted and expert to confirm this fact. |
6/13/2023 6:08 AM | |
Joined: 4/10/2020 Last visit: 11/4/2024 Posts: 77 Rating: (1) |
Thank you very much for your help ! |
This contribution was helpful to1 thankful Users |
Follow us on