8/30/2024 7:48 PM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33840 Rating: (4206)
|
This is not wishful thinking, but perhaps a practical solution. |
9/1/2024 11:10 AM | |
Joined: 6/11/2019 Last visit: 9/26/2024 Posts: 2268 Rating: (99) |
The 0-10V control should not be confused with the 1-10V control. Unfortunately, there are very few converters available to buy for connecting these two active control systems. The only one I know of is the product described in the link. Known DIY solutions have not convinced me so far. Especially since the control voltage from the 1-10V technology is no voltage, but is not considered a protective no voltage. In the event of a fault, it is possible to get the full mains voltage into your log control with a DIY solution. Regards Ella_68 (Translated by google) |
Follow us on