(0)| 11/9/2021 9:03 PM | |
|
Posts: 257 Rating:
|
Hello SIOS Forum Community, It happens that the SIMATIC S7-1200 / S7-1500 are used at very high altitudes. Typical applications are e.g. cable cars, wind turbines, tunnels, automotive plants or mines. Some information is available on this subject: Conversion of the modules of the S7-1500 / ET 200MP for use in installation altitudes above 2,000m Please note the following information in the document, among others !!! The maximum installation altitude for all components is 5000m above sea level. At altitudes > 2000m, the derating factor for ambient temperature must be taken into account. Best regards, SIMATIC International Technical Support Hub |
Follow us on