(0)| 6/23/2022 11:14 PM | |
|
Posts: 5 Rating:
|
hi guys i have a problem with CP CP443-1 that not working and also the CPU OF S7-400 can you help me to investigate and repair this problem thanks |
| 6/24/2022 2:32 PM | |
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello offarbour; You seem to have a number of issues to fix in order to make your system functional. Let's start with the CPU number switches. By the way, how are you warned that the rack number is not correct? When you have a warning message it would be useful for us to see it, sometimes they contain information that we can use to help you out. Take a screenshot of the message and post it here for us to examine. Here is the system manual for S7-400H systems for version 4.5, it should correspond to your S7-417-4H CPUs. https://support.industry.siemens.com/cs/ca/en/view/1186523/26864182283 It will open on the page discussing the hardware setup of the CPUs: look at point 2. "2. Set the rack numbers using the switch on the rear of the CPUs". So power down one power supply remove the CPU and look for the switch behind that CPU. One switch has to be set to 0, thus this CPU will act as primary CPU. Replace it in the rack and power it up. The other CPU must be set as standby its switch has to be set to 1; proceed the same way you did on the primary. Place the second CPU back into the rack and power it up. Tell us if this resolves the rack number issue. If it does, do you now have access to the CPUs over Step 7? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/24/2022 15:01:55 |
|
| 6/24/2022 8:20 PM | |
|
Posts: 5 Rating:
|
Hi bro So now I can connect the PC to the cpu But I can enter ton diagnostic materials Pictures below Thanks |
Last edited by: offabour1 at: 06/24/2022 20:36:25 |
|
| 6/25/2022 3:55 PM | |
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello offabour; If you want to discuss this in French, please use PMs (Personal Messages, look under MyForum in the Navigation bar at the left of this page), not the main forum page, where English has been chosen as an international language. There is also a German section of the forum, if you prefer. First thing, I do not recall you mentionning the ype of connection you want to use between your programming PC and the PLCs. How do you plan to connect in order to transfer the program? There are many ressources you can research both n the frum and on the web, here is an step-by-step example of a Download procedure for a S7-400 CPU with RAM memory card: https://forumautomation.com/t/how-to-connect-and-download-program-to-s7-400/8991 Note that if you are working with a S7-400H system (with RAM memory cards) then all you have to do is to downlaod to the primary CPU as in the procedure, the fiber-optic link between the CPUs will transfer the user program to the standby CPU automatically on the first scan. The main document for creating your user program with Step 7 (v5.x) is this one, Ch. 19 discusses all issues related to Downloading and Uploading the user program, in great detail: - Programmming with Step 7, https://support.industry.siemens.com/cs/za/en/view/109751825 You already have access to the system manual for the S7-400H v4.5 CPUs, for specific information related to the H-system you are working with. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/25/2022 15:57:37Last edited by: dchartier at: 06/25/2022 16:01:05 |
|
This contribution was helpful to
|
|
Follow us on