(0)| 8/30/2022 10:11 AM | |
|
Posts: 1 Rating:
|
i am using iot2040 + I / O card with 5 DI. Need to export /sys/ class /gpio in bash, the appropriate gpio numbers to read the inputs (D0, D1, D2, D3, D4). I can't find out what the numbers are. (these are not values for mraa, I don't want to use mraa, mraa work only as root) For example: bash: echo15 >export python ------------------------------------------------------------------------------------------ |
Last edited by: Przemsonm_ at: 08/30/2022 10:13:00Last edited by: The Helping Hand at: 08/31/2022 12:48:35New subject after splitting |
|
Follow us on