(0)| 10/18/2022 12:04 PM | |
|
Posts: 4 Rating:
|
Hi everyone! I'm Manu, I'm working right now with an IOT 2000 that i need to use it for a task. The software that i use to connect it with my PC it's Node-Red. But i have a problem,node-red don't receive in the log the 1 or 0 outputs. What i want to do it's connect this motion sensor with node red and send the data that i receive when something cross the sensor (we call this "ticks" = product that cross the line of the sensor in a production labeling machine). When something cross it, node-red should detect it like a 0 or 1. The principal error, was that the node that i was trying to install, it was made for a V2.4 image and it was getting an error that it isn't deploy it, like the node appears in the manage palette but i couldn't use it. The node is I solve it(partly), i solved it installing in the SD card of the device a V2.4 image and installing the nodes globally in this one. This is inside Now the problem that i have is it worked all the configuration and installation but the sensor doesn't read me the inputs. I don't know why. I try to use the script I can connect node-red with my database in phpymyadmin buti don't see a "1" in the logs (here is a image) It's like the node don't read nothing and digital inputs don't work. Maybe i have something wrong in the installation or configuration? I can send you whatever you need. Best regards, Manu |
Last edited by: mgoodwork at: 10/18/2022 12:05:12Last edited by: mgoodwork at: 10/18/2022 12:07:01 |
|
Follow us on