11/22/2022 12:57 AM | |
Joined: 3/27/2015 Last visit: 4/2/2025 Posts: 16 Rating:
|
I am having a problem with the fm458. when the machine is working, the fm458 module stops working, all the LEDs are blinking, and the CPU S7-400 also stops working so I can't check what happened. This happens about once every 1-2 weeks. Has anyone encountered this and what is the solution? For information, the FM458 is 6DD1607-0AA2 ,firmware V2.1 Please watch attach video. AttachmentIMG_6375.mov (786 Downloads) |
11/22/2022 3:54 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Hello. Connect directly to the FM458-1DP via DUST1, goto CFC-menu CPU-Module Information and copy from both tabs the diagnostic information. Also try to find inside the conference similiar threads. |
11/23/2022 3:36 AM | |
Joined: 3/27/2015 Last visit: 4/2/2025 Posts: 16 Rating:
|
Can you explain in detail how to connect using dust1 or any document that mentions about connecting FM458 |
11/23/2022 4:55 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Hello. DUST1 is a service protocol, RS232 interface on X1 9-pin sub-D socket. You should connect your PC using RS232-cable to X1 on FM458-1DP, select DUST1 in Setting PG/PC Interface. Manual is here. |
11/25/2022 8:46 AM | |
Joined: 3/27/2015 Last visit: 4/2/2025 Posts: 16 Rating:
|
I will connect to the module when the error occurs again. But is there anything I can do to prevent this from happening? What could be the reasons for this? Why does this issue cause the CPU to stop working? This issue has a major impact on the factory. I hope you can assist. |
11/25/2022 11:02 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Did you try to reprogram MMC offline using USB-Prommer or Field PG as suggested in other similiar threads? |
11/28/2022 5:55 AM | |
Joined: 8/24/2012 Last visit: 7/17/2025 Posts: 4 Rating:
|
I had this issue in multiple occasion in multiple machines. Updating to the latest firmware solved. Operating system updates for FM458-1 DP - ID: 26651134 - Industry Support Siemens The last update that solves the memory card I believe the main culprit for this "All LED Flash" |
Last edited by: Kailasa at: 11/28/2022 05:56:48Last edited by: Jen_Moderator at: 11/28/2022 12:56:30Link optimized. |
|
This contribution was helpful to
1 thankful Users |
1/11/2023 1:36 AM | |
Joined: 3/27/2015 Last visit: 4/2/2025 Posts: 16 Rating:
|
I will try updating firmware, thank you for your reply. |
1/12/2023 1:29 AM | |
Joined: 3/27/2015 Last visit: 4/2/2025 Posts: 16 Rating:
|
I made a direct connection with the FM-458-1 module as your instructions (details in the attachment). But CFC still shows connection error. Can you point out what I missed? |
Last edited by: AutoGen_770497 at: 01/12/2023 01:52:36 |
|
1/12/2023 3:49 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Hello. Can you go online with this program via Simatic CPU interfaces (MPI/DP/IE)? |
Follow us on