(0)| 4/28/2023 8:21 PM | |
|
Joined: 10/30/2022 Last visit: 4/15/2025 Posts: 16 Rating:
|
Dear fellow PCS7 enthusiasts, I came across your discussion as I have a similar problem. I have a PAC4200 meter that uses a RS485 expansion module (slot 2) to connect to a number of circuit breakers. I can connect to the PAC4200 using PowerConfig over ethernet and go live on it, change he settings, etc. I can also connect to it with a Modbus TCP master simulator. However, do you know the proper way of accessing all devices downstream from it? Is there a way to see their registers through a Modbus master simulator connected to the main PAC meter? For example, the IP address of the PAC4200 is 192.168.216.26:502. Also, our Modbus gateway port is 17003. However, how can we set up the PAC, so that an outside device can first connect to 192.168.216.26:502, and then connect to RS485 bus device 2 through gateway port 17003? Thank you for your help in advance, Datigo ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2023 08:50:37New subject after splitting |
|
Follow us on