(2)| 5/8/2024 7:05 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, as already mentioned the firmware of CPUs itself is bound to a specific version of TIA, CPUs can not be configured via GSDML and therefore also not updated via installing a new GSDML. An overview can be seen here: How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?The "additional information" is just a info, it does not cause an error (if the used versions are compatible" which in this case, they are. However, If you use incompatible versions, this message is realted to a error indeed. regars sancruz |
|
Feedback appreciated, please rate |
|
This contribution was helpful to
|
|
Follow us on