6/10/2024 6:49 AM | |
Posts: 4 Rating:
|
Hi, We experience the same problem with a "6es7954-8lc04-0aa0" 4MB memory card. This memory card is the succesor of the "6es7954-8lc03-0aa0" 4MB memory card. The old version of the card is working perfect. When inserting a new card (before power up), the orange LED starts flashing when the CPU is powered. We have tried several new cards en PLC's (CPU215, CPU214), but the all react the same (flash orange LED). With the old version of the card, we have no problems (luckly we have some on spare). Does anyone has an idea what could be the cause and solution for this issue? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/10/2024 11:54:27New subject after splitting |
|
6/10/2024 2:06 PM | |
Joined: 7/7/2010 Last visit: 9/17/2025 Posts: 16110 Rating:
|
Have you prepared the memory card for use as a program card, or to expand load memory, or whatever? The card needs to be prepared for the specific use case. F1-Help and the S7-1200 System Manual describe what the memory card is trying to do. If I recall correctly, the new memory card is basically moving the project from the PLC to the memory card. However, you really should read up on the correct ways to use memory cards in the s7-1200 PLCs. There are many posts in the s7-1200 conference about memory cards. Might be worth a search.
|
science guy |
|
6/11/2024 1:03 PM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, which LED is flashing exactly and are there any other LEDs flashing lighting in which colors (also alternating colors)? Compare that with this table: Status-LEDsIs the LED status not described in the table, create a Support Request. regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
10/24/2024 7:22 AM | |
Joined: 3/2/2020 Last visit: 8/13/2025 Posts: 8 Rating:
|
Hi, I had exactly the same issue with the same status LED. Machine was working but i dont like new machines this kind of warning on the PLC. In the diagnostics i only found a warning with: Maintenance required - Card reader / writer warning Replace to the older now spare-parts SMC (6ES7954-8LC03-0AA0) and all working without LED blinking. Eventually did the firmware upgrade to V4.6.1 and all solved with the newer SMC (6ES7954-8LC04-0AA0) So next time when we have a software update for a existing machine which is not possible to connect via VPN the customer must also update the firmware by SMC. instead of only change SMC with new software and run. (How can you use the memory card for the S7-1200 CPU? - ID: 87133851 - Industry Support Siemens point 6.) But the strange thing for me is the sales and delivery release stated: The SIMATIC memory cards with the new article number are spare part compatible with the previous versions and can be ordered and delivered whith immediate effect.(Sales and delivery release for 4 MB, 12 MB, 24 MB, 256 MB, 2 GB and 32 GB SIMATIC... - ID: 109816058 - Industry Support Siemens ) Hope this helps everybody who has same issue. BR! |
Last edited by: Moderator_Lan at: 10/24/2024 07:54:19links optimized |
|
This contribution was helpful to
1 thankful Users |
Follow us on