(2)| 6/12/2018 7:33 AM | |
|
Posts: 5521 Rating:
|
hi, can you attach the complete diagnostic buffer? I guess some of the entries before can tell us whats up there. regards, |
| 6/12/2018 10:01 AM | |
|
Posts: 12 Rating:
|
Hi, I have attached the diagnostics buffer. Note: Event 1 to Event 11 - 06/11/2018 (During this time only B-CPU becomes Auto Stop & Auto Start) Event 12 to Event 120 - 04/04/2018 (Previous Events) AttachmentCPUA_1515.txt (1035 Downloads) |
| 6/12/2018 10:40 AM | |
|
Posts: 5521 Rating:
|
okay, so there is no hint in the previous entries. in a S7-400H-system the CPU goes into error-search mode, when there is a internal error. this error can be a memory-error, or something like this. When the CPU has checked the error, it is linking up automatically with its partner-CPU. CPU-behaviours in those cases is being improved in FW-Updates.I recommend you to update the FW to the newest version. Operating system updates V6 CPU412-5H PN/DP, CPU414-5H PN/DP, CPU416-5H PN/DP, CPU417-5H PN/DPTo get information what was exactly, you need to contact Siemens with a Support Request. They can read the hex-codes in the diagnostic buffer. hope this helps, regards, |
| 5/6/2024 12:21 PM | |
|
Joined: 12/21/2018 Last visit: 1/6/2026 Posts: 4 Rating:
|
Dear sir, Problem solved or not??? |
| 11/8/2024 9:56 AM | |
|
Joined: 5/24/2022 Last visit: 5/21/2025 Posts: 2 Rating:
|
Dear sir, Your problem is resolved or not ? If resolved how ? Kindly reply |
Last edited by: Notu at: 11/08/2024 09:56:54 |
|
Follow us on