(0)| 11/13/2024 9:52 AM | |
|
Joined: 3/12/2024 Last visit: 1/12/2026 Posts: 231 Rating:
|
Hello, can you please confirm that you have set the boot order correctly:
you can check your current boot order with
to change your boot order please use this command
If you are using Example Image V1.0.2 or V1.1.1 please remove the quotation marks from the command
After changing the boot order please check it again with the above mentioned command. __________ You can also change the boot order in the u-boot-shell using your UART cable:
You can also try to boot specifically from the eMMC with this command in the u-boot-shell:
(this will only affect the next boot) _________ You can try to create your mount-directory on your own:
Please have in mind that Linux is case sensitive so you also need to use "USB" for future-commands:
_________ Your IOT2050 Advanced FS:09 should have an preinstalled IndOS V3.2.3. If you think this is damaged or something you can try to install a new IndOS to the eMMC using a Service Stick. You can download the Instructions for the Service Stick here and you can find the Service Stick Image for V3.2.3 on our Download Page. BR |
Follow us on