(0)| 11/20/2024 3:47 PM | |
|
Joined: 7/4/2012 Last visit: 10/1/2025 Posts: 3 Rating:
|
Hello everyone, I am working on a configuration involving a CU320-2 PN from the SINAMICS S120 range, paired with a Double Motor Module equipped with the Safe Brake Control (SBC) function. My question is as follows: Is it possible to use the Safe Brake Test (SBT) function when the Safe Brake is managed by the SINAMICS system for two motors (with integrated brakes) mounted on the same drivetrain? In this case, it would be necessary to disengage Motor 1 during the test on Motor 2, and vice versa. I hope my question is clear enough. Thank you in advance for your help! Best regards.
https://support.industry.siemens.com/cs/ww/de/view/109763292 |
Last edited by: allyouneed at: 11/20/2024 15:58:11Last edited by: allyouneed at: 11/20/2024 15:58:50Last edited by: Moderator_Lan at: 11/21/2024 07:36:26link optimized |
|
Follow us on