12/2/2024 7:54 AM | |
Joined: 1/5/2018 Last visit: 9/1/2025 Posts: 13 Rating:
|
Hello, I am currently using an S7-1500 PLC with the 6ES7 137-6AA01-0BA0 CMPtP module to communicate with a device via RS-485 using MODBUS. I have encountered synchronization errors when trying to communicate, and I would appreciate your help in troubleshooting this issue. Setup:
Issue:When trying to read from the MODBUS device, I receive the following synchronization errors:
Interestingly, the setup was working fine previously, but now, after replacing the communication module with an identical one (same order number), it starts giving the errors mentioned above. However, when I replace the problematic module with another one of the same type, the communication works as expected. Questions:
Any help or suggestions would be greatly appreciated. Thanks in advance! Attachmentscreenshots.zip (170 Downloads) |
Last edited by: geekpirate at: 12/02/2024 08:08:37 |
|
Follow us on