1/17/2025 10:07 AM | |
Joined: 10/16/2020 Last visit: 9/8/2025 Posts: 146 Rating:
|
Hi! Ensure that your certificates are up-to-date "No connection to the OPC UA server after WinCC Update". Make sure that you have correctly configured the connection parameters, including the security policy and mode "Creating a connection to the OPC UA server". BR |
If this information has been helpful to you, please don't forget to rate it. |
|
1/17/2025 2:30 PM | |
Joined: 1/16/2025 Last visit: 2/2/2025 Posts: 3 Rating:
|
Thankyou for your answer Update my problem 1. New PC Wincc 8.0 (Old PC Install Wincc 7.5 set OPC UA Client and connect KepserverEX OPC UA Server ) 2. New PC Create Certificate from "Wincc Certificate Manager" 3. Install certificate from Kepserver EX position same Old PC 4.When Connect setup "security setting" to None my Connection can Browse Tag But if setup "security setting" to Security Policy : Basic256Sha256,Security mode:SignAndEncrypt ( same Old PC Wincc 7.5) An error occurred while loading the AS Symbols. Note:Unnable to connect to server.Error from server The host name used to connect to a server does not match any host name in the certificate |
1/22/2025 10:17 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello AutoGen_8877347 Check also in the rejected folders if there is a rejected OPC Server certificate in WinCC: https://support.industry.siemens.com/cs/de/en/view/109976723/165322072971 Bye Murof |
Last edited by: Murof at: 01/22/2025 10:18:34If this Information really helps, you could use the Rate function |
|
1/22/2025 2:05 PM | |
Joined: 1/16/2025 Last visit: 2/2/2025 Posts: 3 Rating:
|
Thankyou No Certificate in root rejected For Certificate from "Wincc Certificate manager" I'm not sure to install in root 1.CA = certificate authority root C:\Program Files(x86)\Siemens\WinCC\opc\UAClient\PKI\Issuers\cert 2.CRL = Certificate Revocation List root C:\Program Files(x86)\Siemens\WinCC\opc\UAClient\PKI\Issuers\crl 3.OPC UA client certificate root C:\Program Files (x86)\Siemens\WinCC\opc\UAClient\PKI\OPCUA\certs 4.OPC UA Tags Importer certificate root C:\Program Files (x86)\Siemens\WinCC\opc\UAClient\PKI\OPCUA\certs Befor Install in root I'm install certificate in the Trusted Root Certification Authorities store |
Follow us on