11/28/2022 10:00 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4110 Rating:
|
Hi Karri_R, for a safety-related IO-Controller-IO-Device communication transfer areas with 6 and 12 bytes are needed, see "Safety-related IO-Controller-IO-Device communication - Limits for data transfer". You should also take care to write the parameter LADDR of SENDDP and RCVDP for a S7-300 in hexadecimal format. Kind regards |
This contribution was helpful to
1 thankful Users |
11/28/2022 11:16 AM | |
Joined: 6/7/2016 Last visit: 4/8/2025 Posts: 5 Rating:
|
The communication is now working after adding 6 bytes for both directions. Thank you Stefan Arcularius! |
Follow us on