6/17/2021 3:12 PM | |
Joined: 12/2/2011 Last visit: 6/10/2025 Posts: 3 Rating:
|
Hi everyone! I need to do this configuration in my application. I am using a 1512 (TIA V16) controller, a Modbus-RTU/TCP-IP converter (not gateway, only medium converter) and I have a Modbus-RTU Slave at the serial side. The converter I am using does not have any GSD file to install, then I created a TCP connection between the controller and the converter. The block Modbus_Comm_Load need a hardware identifier at the pin PORT. There's any way so I can configure the block to read slaves data? BR from Brazil ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/18/2021 10:58:43New subject after splitting |
|
6/17/2021 11:52 PM | |
Joined: 12/2/2011 Last visit: 6/10/2025 Posts: 3 Rating:
|
HI, Duris_I! Thanks for answering. I never used a converter like this before, so I'm trying to learn it. I probably wasn't very clear about the scenario. I'll answer you point by point: 1. I created a TCP connection to the converter trying to estabilish communication between the controller and the converter. I thought that, once I need to communicate with a Modbus-RTU slave at serial side, at the controller side I needed to use MB RTU blocks. I dont know if this is the right way to do it. (Probably not XD) 3. Thats what I dont know how to do correctly. How to configure hardware correctly at TIA application and which blocks should I use at my program to set this communication right? Thanks, again. AttachmentUser Manual.pdf (688 Downloads) |
Follow us on