(0)| 3/19/2025 9:51 AM | |
|
Joined: 7/11/2024 Last visit: 12/26/2025 Posts: 200 Rating:
|
Hello Bibek007 This error may be due to a corrupted ALM database. You could try the following: - Unistall the ALM and make sure to delete almdb.sdf file (usually under C:\ProgramData\Siemens\Automation\AutomationLicenseManager\logging\). Then, install it again - Try reinstalling WinCC. To uninstall it properly follow this section of the manual: Uninstalling WinCC. Also, I recommend you to store the license keys to avoid losing them (ALM manual) and to backup the project (How do you do a data backup of the WinCC Project (WinCC V7 and WinCC Professional) on the Operator Station (OS)? Good luck! |
|
If this post has been useful, don't forget to rate it!😊 |
|
| 3/19/2025 12:46 PM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello Bibek007 Please check at first if your WinCC version is compatible with the used OS: https://support.industry.siemens.com/cs/de/en/view/64847781 Which SP do you have installed in your WinCC V7.0? not every SP is compatible with Server 2008 R2 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on