(0)| 6/1/2022 8:22 PM | |
|
Joined: 1/10/2020 Last visit: 11/7/2025 Posts: 25 Rating:
|
hi, i have a simatic hmi tp1200 comfort, the screen freezes on boot with the text "SIMATIC HMI" i can't communicate in any way, is there a way via MMC or USB? I tried them all through prosafe, the problem is that no network device works, so it is impossible to communicate with the pc. I think the only way is something local on the motherboard, so I was asking for a usb or mmc key. maybe a hardware reset could help too, of course I don't know how this can be done, but I think every motherboard has it. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/02/2022 06:08:52New subject after splitting Last edited by: domenico2020 at: 06/02/2022 17:10:56 |
|
| 6/3/2022 8:00 AM | |
|
Joined: 2/17/2020 Last visit: 1/16/2026 Posts: 1251 Rating:
|
Unless the HMI port is damaged, connecting via ProSave should be possible to perform the reset. Try to follow this FAQ and don't forget to configure the PG-PC Interface of your PC, defining the access point as the network card through you use to communicate.TCPIP.1. |
|
A rating will be well appreciated. |
|
| 4/4/2025 4:56 PM | |
|
Joined: 4/4/2025 Last visit: 4/5/2025 Posts: 1 Rating:
|
Hello. I have a similar problem with the tp1200 comfort panel.Did you manage to solve the problem with the panel? |
Follow us on