4/16/2025 12:06 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello evanbp yes the new FW could be tricky. Seems to be OK from the first view... Here is a FAQ for Unified. Also if you do not have unified you can try the different steps in the FAQ: https://support.industry.siemens.com/cs/de/en/view/109955142
If you use WinCC V7/8 for example then you have to so the export with SCADA Export Tool and import it in the WinCC project to get the new certificate (even if you do not use it...) Which HMI do you use? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on