(0)| 1/20/2016 1:05 PM | |
|
Posts: 13 Rating:
|
Hi all, I have version of PCS 7 Version 7.1 SP2. My problem is the communication loss with redundant server (see image attached to the network configuration), as well as, loss of configuring a client (client 3). After successfully loading the OS Server 1 (MASTER), realized the loading OS_Stby to Server 2. Could not finish the charging event of an error (see LOAD.LOG file attached). After that, I called myself to Server WINCC 2 and appeared the error attached. The same happened when the client 3 loading attempts (see LAD.LOAD_Cliente3). View the settings on WINCC Runtime 7.0 SP2 How i can recover my redundant server(SERVER2)? How i can do the download for Client(Cliente 3)? Best Regards
Attachmentfiles.rar (200 Downloads) |
Follow us on