Industry Online Support
Technical Forum
3/7/2006 3:26 PM | |
Posts: 7 Rating: (0) |
Dear Sir/Madam, I have a quick question regarding the TS-adapter and the interface to which it is to be connected. The manual says that is to be connected to the MPI/DP interface...so my question is this: Our plant has an S7-314 CPU (6ES7314-1AF11-0AB0), and to establish a remote connection we have connected a TS-adapter (and a GSM-modem) to its MPI-interface. Now, is this CPU capable of communication via the TS-adapter? I wonder because the manual said "connect to MPI/DP" and the 314 CPU only has a MPI-interface. Best regards Patrick Geiryd patrick.geiryd@benima.se Stockholm, Sweden |
3/9/2006 1:00 AM | |
Posts: 11 Rating: (0) |
Hi, in my plant we have a 314+Ts-adapter and works nice. [:)] Regards |
3/9/2006 12:22 PM | |
Posts: 7 Rating: (0) |
Hi notricks, Thanks for your reply! Best regards Patrick Geiryd |
3/13/2006 10:57 PM | |
Posts: 1 Rating: (0) |
I, any one khnows applcations with TSII and GPRS connection? Many tanks Balboons |
Follow us on