7/31/2025 6:23 AM | |
Joined: 8/3/2009 Last visit: 9/18/2025 Posts: 16452 Rating:
|
Hello AutoGen_783642 The only chance for this exact topology would be S7 routing but this will not work with TIA V20, because you would need PLC Proxy device of your PLCs from the Step7 Project in TIA. But With V20 you cannot work with a Proxy PLC out of a Simatic Manager Project. With V19 it should work: https://support.industry.siemens.com/cs/de/en/view/73502293 (Chapter 3.7) If you have to use TIA V20 then you can only use direct connections like Ethernet with CPs or MPI/DP with also a CP but on PC side Bye Murof |
Last edited by: Murof at: 07/31/2025 06:23:36If this Information really helps, you could use the Rate function |
|
Follow us on