9/12/2025 7:28 PM | |
Joined: 1/21/2013 Last visit: 9/19/2025 Posts: 4114 Rating:
|
Hi Furkanayeng, No, the internal storage cannot be used for logging purposes. Therefore, only external storage devices are possible. Unfortunately, I can't find this information in the documentation. However, the Unified Comfort Panel documentation states that only the SD card and USB interfaces can be used. Since the Basic panel has a reduced feature set compared to the Comfort panel, it is reasonable to assume that the Basic panel does not support internal storage either. Kind regards |
Follow us on