(0)| 11/17/2025 9:14 AM | |
|
Joined: 8/14/2020 Last visit: 12/10/2025 Posts: 333 Rating:
|
Hello miluk1 I suspect your original WinCC flexible project contains custom controls (OCX). There's an FAQ on this topic: https://support.industry.siemens.com/cs/us/en/view/37022154 When migrating a flexible project, OCX controls are not migrated. To use them in the migrated project, you need the source code of the OCX control. As described in the link above, it's necessary to register it in Windows so it can be used in the flexible project. Do you still have the old system where the original flexible project worked correctly? If so, you can check there whether custom controls were used. Best regards, Costanza |
Follow us on