3/24/2009 4:44 PM | |
Posts: 2 Rating:
|
Is it possible to connect an OP7 to PC via converter RS232<>USB ? Thanks |
3/24/2009 4:50 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear yan_alp73, It is not possible Have a look at this link: http://support.automation.siemens.com/WW/view/en/13904923 Best regards, Wizard |
3/24/2009 4:56 PM | |
Posts: 2 Rating:
|
thanks and with a card PCMCIA with RS232 ? |
3/24/2009 5:12 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, I think the answer is also Not possible. But if you have it, try and post the result here. regards |
10/15/2009 9:04 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed inthese threads WinCC Flexible OP7. Problem downloading (--- PANEL OP 7 ---). CANNOT DOWNLOAD PROGRAM FROM LAPTOP TO OP3. Simatic OP 27 and PC. Please continue to discuss in the last mentioned thread. Best regards O_Moderator |
Follow us on