(0)| 4/2/2007 11:52 PM | |
|
Posts: 271 Rating:
|
Walter, Perhaps the attached section in our 611U Function Manual will aid you. My recommendation would be to disable and enable the drive using the Profibus signals first and use the hardware enables only when you have to. I would encourage you to use the 611U Toolbox as well and make use of FB83 a custom function block which makes operation of the 611U very painless. Hope this helps... AttachmentPages from FBU.pdf (698 Downloads) |
Follow us on