(0)| 3/4/2010 7:59 AM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
Hello, here you can download the CX32 FAQ http://support.automation.siemens.com/WW/view/en/28879180 In Capter 5 is a description how to connect the parameters for transfering the infeedready signal. The parameter p8500 is a internal parameter on the CU of the D435 an will be connected automativ from the FW, you must only connect the signals on the CX32 side. The faults of the TM54F can read via ReadDriveFaults with the do number of the TM54F in the command parameters. Regards Christoph |
| 3/4/2010 10:49 AM | |
|
Posts: 3 Rating:
|
Thank You very much for fast and helpfull response. |
Follow us on