(0)| 9/8/2010 11:22 PM | |
|
Posts: 8 Rating:
|
Hello to every one. can i expand the module of logo more than seven expansion module DM8. Because i like to make a project traffic light control in logo |
| 9/9/2010 11:31 AM | |
|
Posts: 173 Rating:
|
Like Helmut said, a SINGLE LOGO! can only control a maximum 24 digital inputs and 16 digital outputs inside its own program. BUT it is possible to join 2 x LOGO!s together with some clever digital I/O signalling between them to get up to 27 digital outputs. Expanding on this idea, you might be able to get more. I supose it depeends if you are wanting the 7 x DM8 to have more inputs or more outputs (more then likely OUTPUTS are needed). So I think you want: 4 + (7 x 4) = 32 outputs. Have a look at the attached progam idea where 2 x LOGO!s are joined with the last 4 outputs of LOGO! #1 connected to 4 inputs of LOGO! #2. You will have to be careful if you want more than 1 output switched at a time - you will need to 'latch' then 'unlatch' them: on both sides. Maybe this will help!?!?!? Cheers AttachmentUp_to_27_Outputs.zip (440 Downloads) |
This contribution was helpful to
|
|
Follow us on