(0)| 1/27/2011 4:24 PM | |
|
Posts: 3 Rating:
|
Thanks for your help. I have another questions. If I use two CPUs for two different machines, can the CPUs share one HMI, like the KTP600? Splitted from S7. |
Last edited by: O_Moderator at: 1/28/2011 11:23 AMnew subject after splitting |
|
| 1/27/2011 4:43 PM | |
|
Posts: 28 Rating:
|
hi Pwong Yes its possible for multiple CPU's to communicate with a single HMI application. check out these links posted by ''how come'' in one of the older posts. 1] MP377 WITH CPU412-3H CONTROLLERS 2] COMMUNICATION OF S7 400 H CPU WITH MP 377 THROUGH ETHERNET LINK 3] How do you connect an operator panel (WinCC flexible) to an H system (S7-400H) about MPI or PROFIBUS? 4] How can you connect an operator panel directly to an H system without using repeaters? 5] WinCC 7.0 and ethernet connection to S7-400 by CP 1613 A2 card |
Follow us on