(0)| 8/1/2011 11:51 AM | |
|
Joined: 2/10/2010 Last visit: 4/16/2025 Posts: 35 Rating:
|
I want to control drive A by torque from an analog input with open speed loop. Only axe A is active (P0700 = 1 for axe A, P0700 = 0 for axe B). I parameterized an analog inputs (Figure 12) and digital inputs (Figure 13) according to SimoComU help and Simodrive 611 manual. The drive does not respond to an analog input voltage. Speed loop is active, as diagnostic message says. Digital input is not active in Terminal simulator mode (gray color) (Figure 11). Could the reason hiding in the wrong setting of some parameter, which blocks torque control abilites? Some information chapters from Help, what I used:
Please, look on attached pictures. With best regards, Maxim Attachmentpictures.zip (491 Downloads) |
Follow us on