(0)| 2/1/2007 12:29 PM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, regarding to your inquiry we would like to inform you. Please see our example program with STEP 7 together with CFC which this is a connection with UDT-Variable. We can not reproduce your described problem. See also the FAQ of CFC-connections http://support.automation.siemens.com/WW/view/de/15350578 It is possible that there are not enough space of your hard disk and/or virtual work memory. We recommend to check the hard disk and the virtual work memory and see in this case the FAQ: http://support.automation.siemens.com/WW/view/de/20440472 Otherwise it is possible that this is a software (STEP 7, CFC, ...) which is not compatible with the operating system Windows. See in these case also the following FAQs: http://support.automation.siemens.com/WW/view/de/8250891 http://support.automation.siemens.com/WW/view/de/18734363 With best regards AttachmentCfc_udt.zip (950 Downloads) |
| 2/1/2007 4:19 PM | |
|
Posts: 20 Rating:
|
Thanks a lot for your reply. I tried all of your suggestions but I think this is something with the CFC editor. I'm actually using all the latest versions of the simatic products. The behaviour seems to happen with the version 6.1 SP1 HF4 and also with the new version 7.0. AttachmentIssue Steps.zip (973 Downloads) |
Follow us on