3/22/2013 11:34 AM | |
Posts: 13 Rating:
|
dear expert, from which D7-SYS version, CPU551 (6DD1600-0BA2) can work? and for all the firmware/version, can the CP50M1 work on D7-SYS V6.2 + SP3? thank you! Wang |
3/22/2013 12:12 PM | |
Joined: 8/25/2006 Last visit: 9/16/2025 Posts: 2218 Rating:
|
Hello. There are no restrictions on D7-SYS version, it may be used with any version of D7-SYS. If you didn't see new CPU551 in HWCatalog, then configure it as6DD1600-0BA2. New TDC CPU551 Released for Delivery
There are only restrictions of using CP50M1 with D7-SYS V7.0 and higher: With D7-SYS 6.2+SP3 you may use CP50M1 with any HW Release/FW version. |
Last edited by: KSN at: 3/22/2013 12:12 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on