7/26/2013 8:53 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello syd_b, I guess you already have seen this faq: how can you set up a connection between a LOGO! 0BA7 and an HMI Panel? You will have to use driver "S7-200", so you can also use WinCC flexible to program the panel. You can use any panel with Ethernet interface and a "S7-200 driver" Best regards, Wizard |
7/26/2013 9:52 AM | |
Joined: 11/23/2011 Last visit: 9/3/2025 Posts: 202 Rating:
|
Hello syd_b, you can have a look on the following two recently released completed application examples for LOGO! 0BA7 in connection with an HMI panel: http://support.automation.siemens.com/WW/view/en/68585344 http://support.automation.siemens.com/WW/view/en/68585346 In each link when you scroll down there is an example code for LOGO! and the HMI panel as well as a documentation where the necessary settings that have to be set for an successfull communication of LOGO!, the HMI panel and your PC are shown. When you have further questions don't hesitate to ask. Greetings, KM_AS |
7/26/2013 10:28 AM | |
Posts: 2930 Rating:
|
Hi, you can find a simple step by step instruction and a complete example wor WinCC flex hier: www.siemens.com/logo --> Application examples Hope this helps |
8/16/2013 12:42 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
Follow up question published by erkuis split to a seperate thread with the subject Problem when HMI menu was time to ask active (default) and LOGO read encoders rapid pulses. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on