10/11/2007 10:41 AM | |
Posts: 25 Rating:
|
Sorry to All I have a mistake, it's not OP27, it is OP270. |
10/11/2007 11:12 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello blondy, When you have OP270, it's possible to programm it with Protool or WinCC flexible. When you want to download it to panel. The panel should have the right image. So it could be possible, you should first update OS. See following link: http://support.automation.siemens.com/WW/view/en/19701610 When you have WinCC flexible 2007, the Authorisations on panel wouldn't be lost. But when you have WinCC flexible 2004 or 2005, you should first remove any possible authorisations from panel. http://support.automation.siemens.com/WW/view/en/22778339 http://support.automation.siemens.com/WW/view/en/22777582 Best regards, Wizard |
Follow us on