(0)| 1/25/2016 6:46 AM | |
|
Posts: 8092 Rating:
|
Hello, This is 611-Analog drive, 80/160 A enhanced interface feed module. If fault is sporadically reset it or if it is permanent, significance of fault code 7 is motor feeder cable interrupted or motor cable short circuit or ground fault etc. If every thing is Ok, then control module is faulty, replace the same. Please refer attached sheet. |
| 1/26/2016 8:18 PM | |
|
Posts: 50 Rating:
|
Thanks for the help, the drive was the cause of the fault. |
This contribution was helpful to
|
|
Follow us on