12/15/2016 11:34 PM | |
Posts: 5225 Rating:
|
I am going to try something new. Please find attached a ZIPPED video file. I recommend using VLC to play the file. AttachmentMovie_Define hardware interrupt.zip (667 Downloads) |
This contribution was helpful to
1 thankful Users |
12/16/2016 5:13 PM | |
Joined: 4/9/2010 Last visit: 7/4/2025 Posts: 236 Rating:
|
I just happened to have the hardware and some free time to apply all the valuable advice I enabled HSC1 and accepted the default reset signal to be connected to I0.3, set input fliters of all three signals to minimum, checked the "Generate interrupt for external reset event" and accepted default name "Hardware interrupt" for Hardware interrupt OB. Works like a charm.By the way, it is not necessary to use the physical input inside the interrupt since the interrupt itself is triggered by that input. Hopefully the enclosed project will help Jakob. Regards, Adam AttachmentHSCTest.zip (672 Downloads) |
This contribution was helpful to
1 thankful Users |
12/16/2016 7:37 PM | |
Joined: 4/9/2010 Last visit: 7/4/2025 Posts: 236 Rating:
|
William, Is the enclosed program what you had in mind? Regards, Adam AttachmentHSCTest1.zip (681 Downloads) |
Last edited by: adam_ski at: 12/16/2016 9:24:33 PMLast edited by: adam_ski at: 12/16/2016 9:25:41 PM |
|
12/20/2016 4:51 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
Never |
Follow us on