(0)| 6/4/2017 7:46 PM | |
|
Posts: 32 Rating:
|
Hello , I am having issues installing the MRAA library, this hangs with the error "ValueError: semaphore or lock released too many times". The full log of this install is included below. The other issue is with installing Mosquito. I am getting an issue with clock skewing resulting in the build not being completed. I have included a file below that has the full output of two install attempts (make WITH_SRV=no) followed by an attempt to built (make test). If you could help me resolve these issues i would be very appreciative. Thankfully Kas root@iot2000:~/.node-red# npm install mraa > mraa@1.7.0 install /home/root/.node-red/node_modules/mraa > node-gyp rebuild make: Entering directory '/home/root/.node-red/node_modules/mraa/build' make: Warning: File '../binding.gyp' has modification time 3611765 s in the future ACTION Regenerating Makefile Process PoolWorker-1: Traceback (most recent call last): File "/usr/lib/python2.7/multiprocessing/process.py", line 258, in _bootstrap self.run() File "/usr/lib/python2.7/multiprocessing/process.py", line 114, in run self._target(*self._args, **self._kwargs) File "/usr/lib/python2.7/multiprocessing/pool.py", line 102, in worker task = get() File "/usr/lib/python2.7/multiprocessing/queues.py", line 380, in get rrelease() ValueError: semaphore or lock released too many times make[1]: warning: Clock skew detected. Your build may be incomplete. make[1]: Leaving directory '/mosquitto-1.4.12/src' set -e; for d in man; do make -C ${d}; done make[1]: Entering directory '/mosquitto-1.4.12/man' make[1]: Warning: File '../config.mk' has modification time 5022797 s in the future make[1]: Nothing to be done for 'all'. make[1]: warning: Clock skew detected. Your build may be incomplete. make[1]: Leaving directory '/mosquitto-1.4.12/man' make: warning: Clock skew detected. Your build may be incomplete. AttachmentMQTT Install Issue.txt (517 Downloads) |
Follow us on