6/19/2017 10:42 PM | |
Posts: 6 Rating:
|
Dear All, I would like to ask about task scheduler like cron. What is substitute of missing cron service in Yocto Linux iot2040? |
6/20/2017 9:57 AM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
None is pre-installed, but we can add cronie to the next release. Already pushed https://github.com/siemens/meta-iot2000/commit/00826acf00a4158a73be2f9b198d859329dcfe26 and tested this lightly on the device. You can build your own image, see also https://support.industry.siemens.com/tf/ww/en/posts/building-fresh-iot2000-sd-card-image-via-a-single-command/168681/?page=0&pageSize=10 |
This contribution was helpful to
1 thankful Users |
6/20/2017 1:38 PM | |
Posts: 6 Rating:
|
Thx, Would be great to have such scheduler in standard like regular Linux. |
7/2/2017 11:02 PM | |
Joined: 2/14/2017 Last visit: 4/17/2023 Posts: 59 Rating:
|
If you're able to build the SD card image from the instructions above, here are the steps I used to add cron to it: |
Follow us on