(2)| 6/2/2008 10:29 AM | |
|
Posts: 2 Rating:
|
Can anybody help for Simodrive configuration and Simatic Manager settings for Profibus settings? |
| 6/2/2008 11:22 AM | |
|
Posts: 17 Rating:
|
Hi, It is not easy to write all steps. What have you done? |
| 6/2/2008 10:28 PM | |
|
Posts: 271 Rating:
|
Hello Jaypee, First off, the documentation is available at www.automation.siemens.com/doconweb for the 611U control unit. I encourage you to download the 611U Toolbox available at the following web site: http://support.automation.siemens.com/WW/view/en/29055038 Included is a sample project that will allow you to operate the 611U positioning control unit as a basic positioner utilizing the traversing blocks. The toolbox includes an explanation of the special function block FB83 for use with 611U drives. The telegram type typically used is 110 and the MDI mode is made available to you for large motion profiles. Hope this helps... |
Follow us on