(0)| 1/27/2017 1:42 PM | |
|
Posts: 100 Rating:
|
Hello, so no way to simulate, thanks for your help Moelsayed |
| 1/9/2019 9:30 AM | |
|
Posts: 27 Rating:
|
WinAC is the delicate PLC so you simply need to make a step7 program in it include the station and do the equipment config include the WinAC and the system card to it give appropriate ip address and afterward in the other PC open the WinAC PLC board in which you have introduced WinLC RTX and open station config include the rtx and netwaork card to it and after that download the stage 7 program it from the fundamental PC Presently the WinAC PC will go about as a real PLC
|
Follow us on