(0)| 11/11/2008 9:09 AM | |
|
Joined: 10/7/2005 Last visit: 1/15/2026 Posts: 3054 Rating:
|
Hello idunnohow I'm not to sure if your OP37 was really configured with proTool V1.x (OP37 can only be configured fromProTool V3.x onwards, see here for more on this: http://support.automation.siemens.com/WW/view/en/28735883) But if you really do have a ProTool V1.x configured project, theFAQ below should help (link: http://support.automation.siemens.com/WW/view/en/213253) QUESTION: ANSWER: |
|
Cheers |
|
| 11/11/2008 9:15 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hi Did you try with Prosave to make backup of OP37? And are you sure that program into OP37 is made by Protool 1.x? See this FAQ: Which Engineering Software can be used with which panels? And when try to open what kind of error you receive? regards |
Follow us on