(0)| 12/2/2019 11:21 PM | |
|
Joined: 6/20/2014 Last visit: 8/21/2025 Posts: 21 Rating:
|
Hi, I need help with FM458, my issue is the following : NAV block has QFC:=1 and YFC 16#0001, but PR, RS, or RP are different than Zero, here attached a print screen. (from CFC Help : YFC bit 1 Configuration error: At least one of the inputs PR, RS, or RP is set to 0.). The encoder name in HW configuration is same as in CFC Project , 5v type and DIP switches set correctly. X438_1 connected correctly using X2 with SC63 cable from SU13 (i.e. Encoder 2 : Pins 26,27 28,29 30,31. Regards. YB ------------------------------------------------------------------------------------------ AttachmentFM458_Encoders.zip (748 Downloads) |
Last edited by: Jen_Moderator at: 12/03/2019 10:11:33New subject after splitting |
|
Follow us on