(0)| 12/9/2020 6:05 PM | |
|
Posts: 22 Rating:
|
Hi, I am trying to restrict SSH access to only X1P2 (192.168.200.1) port which is connected to a local PLC network and block all connections on X1P1 (dhcp/static) port which is used to connect the IOT2050 to the internet. I don't want the device publicly accessible via SSH through Internet hence X1P1 SSH blocking is required. I did google and came across this article which does the trick: Restrict SSH to one interface However, it works after making the modification and restarting the SSH service. However, after a reboot of the IOT device, all SSH connections are blocked both on the X1P2 and X1P1 port (very strange). However, I have to restart the SSH service every time. Is there a fix or a better way to do this? It seems like the settings made in SSHD_config file are not updated after a device restart.
Thanks, Nisarg
|
| 12/10/2020 3:45 PM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello Nisarg, Thanks a lot for your tests, we will have a deeper look into this! An unelegant solution for now would be to run a script at startup to restart the ssh service? You could use crontab for this. The most elegant solution on the other hand would be to block port 22 on eth1 using a firewall (iptables/nftables) but in this case we would need a fresh image based on the master-branch, as we would require some underlying fixes that were commited after the Example Image V1.0.2 Release. Best regards!! |
| 12/15/2020 12:39 PM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello Nisarg, Do you mean the crontab or your restart command is not working? Maybe the ssh service takes a while to start.. You can try adding the script in the attachment to the base directory of your IOT and then editing the cronjob like this: Notice that the script will also create a file in your user directory. How have you been testing the sytemctl command before? Over FDTI cable? For me this command results in a timeout if I'm simultaneously connected over SSH. BR Attachmentssh-restart.zip (636 Downloads) |
Last edited by: Fe_lipe at: 12/15/2020 12:39:41 |
|
Follow us on